What if USB interface is not populated over Target board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What if USB interface is not populated over Target board

958件の閲覧回数
adityanagal
Contributor III

Hi ,

What I understood from the IMX6 reference manuals , In the bootstrap mode host and ROM communicates over serial download protocol over USB interface for flashing Uboot , kernel etc on boot device . What if the USB interface is not

populated over the target board. Then is there any way to flash the uboot , kerenel etc on boot device.

Please suggest.

0 件の賞賛
返信
2 返答(返信)

884件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Aditya,

if you are not using the USB then you can use the UART to download the code, but it is extremely slow a comparison with the USB port.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

884件の閲覧回数
adityanagal
Contributor III

Hi ,

How to use the UART instead of USB in Serial Download booting mode for firmware flashing . Is it possible to use UART in Serial download mode for firmware flashing ?

Regards,

Aditya Nagal

0 件の賞賛
返信