What features are supported by the i.MX MFG Tool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What features are supported by the i.MX MFG Tool?

2,443件の閲覧回数
chetkaufman
NXP Employee
NXP Employee

My customer is wondering if the following functions are supported by the MFG Tool as they plan to set it up for high volume board programming.   This will be on i.MX7 Dual platform.

Flash eMMC

Install Public Keys

Set to shipping mode

Retrieve CPU ID

Write to fuses

Load data into RAM

ラベル(2)
0 件の賞賛
返信
7 返答(返信)

2,022件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chet

one can check *.vbs files (search for "7D") in folder  latest i.MX Series Manufacturing Toolkit for Linux 4.9.11_1.0.0 Release

https://www.nxp.com/webapp/Download?colCode=IMX6_L4.9.11_1.0.0_MFG_TOOL&appType=license&location=nul... 

Seems supported programming eMMC, SD, SPI-NOR, NAND, QSPI-NOR, WEIM-NOR.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,022件の閲覧回数
chetkaufman
NXP Employee
NXP Employee

Thanks Igor.   Can you also answer if the MFG Tool can do the following actions:

Install Public Keys

Set to shipping mode

Retrieve CPU ID

Write to fuses

Load data into RAM

0 件の賞賛
返信

2,023件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chet

I am afraid they are not supported.

Best regards
igor

0 件の賞賛
返信

2,023件の閲覧回数
chetkaufman
NXP Employee
NXP Employee

Igor,

   Please review this again.  I know the MFG Tool can be used to write to the e-fuses.   I need confirmation this applies to the Public Keys.  See the blog post here:

Burning eFuses on i.MX6 and i.MX7 - i.MXDev Blog 

I also need to know if it can be used to:

Retrieve CPU ID

Load data into RAM

0 件の賞賛
返信

2,023件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chet

 

yes it can be used in theory, but default mfg tool should be modified for these additional features.

 

Best regards
igor

0 件の賞賛
返信

2,023件の閲覧回数
chetkaufman
NXP Employee
NXP Employee

OK thanks Igor.    Can you confirm how my customer should modify the MFG Tool to enable these additional features?

0 件の賞賛
返信

2,023件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chet

customer can apply to NXP Professional Servicesto develop these features:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE
alternatively you can enter ticket on application team link : community.nxp.com/groups/imx-support/

based on available resources and customer project additional help may be provided.

Best regards
igor

0 件の賞賛
返信