What do do with unconnected DDR3 balls in a 32-bit configuration of iMX6Solo?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What do do with unconnected DDR3 balls in a 32-bit configuration of iMX6Solo?

跳至解决方案
1,584 次查看
emil
Contributor III

Hello,

Since the iM6Solo only supports 32-bit memory bus, but have balls for a 64-bit memory bus it is unclear to me how I should connect these 32 unused balls. Should they just be left unconnected?

Thanks!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,380 次查看
Yuri
NXP Employee
NXP Employee

Unused signals / pins of 64-bit memory I/F (in 32-bit mode) may be left free,

as stated  in section 5 (DRAM interface requirements for migration) of app

note AN4397 (Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite)

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,381 次查看
Yuri
NXP Employee
NXP Employee

Unused signals / pins of 64-bit memory I/F (in 32-bit mode) may be left free,

as stated  in section 5 (DRAM interface requirements for migration) of app

note AN4397 (Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite)

0 项奖励
回复