What do do with unconnected DDR3 balls in a 32-bit configuration of iMX6Solo?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What do do with unconnected DDR3 balls in a 32-bit configuration of iMX6Solo?

ソリューションへジャンプ
1,589件の閲覧回数
emil
Contributor III

Hello,

Since the iM6Solo only supports 32-bit memory bus, but have balls for a 64-bit memory bus it is unclear to me how I should connect these 32 unused balls. Should they just be left unconnected?

Thanks!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,385件の閲覧回数
Yuri
NXP Employee
NXP Employee

Unused signals / pins of 64-bit memory I/F (in 32-bit mode) may be left free,

as stated  in section 5 (DRAM interface requirements for migration) of app

note AN4397 (Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite)

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,386件の閲覧回数
Yuri
NXP Employee
NXP Employee

Unused signals / pins of 64-bit memory I/F (in 32-bit mode) may be left free,

as stated  in section 5 (DRAM interface requirements for migration) of app

note AN4397 (Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite)

0 件の賞賛
返信