What could be causing the SPI bus Linux Driver, not to function on iMX6Q.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What could be causing the SPI bus Linux Driver, not to function on iMX6Q.

2,344件の閲覧回数
michaelbrainerd
Contributor I

I am writing an application to Stream video over SPI from a Veriscite DART SOM, to a ARM Cortex-M3.

The Linux image is Yocto Krogoth:

this is the kernel error message:

  • spi_master spi0: cannot find modalias for /soc/aips-bus@02000000/spba-bus@02000000/ecspi@02008000/ecspi1grp
  • spi_master spi0: Failed to create SPI device for /soc/aips-bus@02000000/spba-bus@02000000/ecspi@02008000/ecspi1grp
  • spi_imx 2008000.ecspi: probed
ラベル(4)
0 件の賞賛
返信
1 返信

1,854件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michael

some boards may have pin conflicts ecspi1 with other modules, like imx6qdl-sabreauto.dtsi :

linux-2.6-imx.git - Freescale i.MX Linux Tree 

so one carefully check ecspi1 muxing options

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信