Hello Rasmus,
1. Is there a similar DDR3 script aid available for i.MX7D that exists for i.MX6?
ANSWER. Yes, we have but it is only for Internal Use Only, since it is under development. If you want more details please enter a CASE, so we can discuss it in private.
Is the script provided with the tool "MX7D_DDR3_register_programming_aid_v09.ds" actually valid for the SABRE development board? - If so, then it's probably also valid for us, since the memory design is based on SABRE.
ANSWER. Yes, it is valid.
3. After the calibration, is it enough to enter these two values into the U-Boot configuration file (like here: git.denx.de Git - u-boot.git/blob - board/freescale/mx7dsabresd/imximage.cfg ) registers DDR_PHY_OFFSET_RD_CON0 (0x30790020) & DDR_PHY_OFFSET_WR_CON0 (0x30790030)?
ANSWER.The DRAM controller IP in MX7D is different from the MX6 series MMDC controller. Results from DRAM calibration may be updated for the following registers: DDR_PHY_OFFSET_WR_CON0 (0x30790030) and DDR_PHY_OFFSET_RD_CON0 (0x30790020). Also, the MX7D memory map DRAM starting address is fixed at 0x80000000.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------