What addresses are the IMX7D integrated power switch registers mapped to?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What addresses are the IMX7D integrated power switch registers mapped to?

461件の閲覧回数
takayuki_ishii
Contributor IV

Hello community,

 

Our product is a battery-powered portable device.

We do not use Linux BSP but ROTS for this product.

 

In this product, some i.MX7D devices have a very large VDD_SOC leakage current

during power saving, resulting in a very short standby time.

So we plan to control SW_SOC_PD switch.

 

In following community thread, it say that 

please refer to section 5.5.11 (GPC PGC Memory Map/Register Definition) of i.MX 7Dual Applications Processor Reference Manual, Rev. 0.1, 08/2016

How to control the i.MX7D integrated power switches ON/OFF 

 

However, while the six switches and corresponding registers can be guessed, SW_SOC_PD and SW_FUSE are not clear.

Q1. Is the ON/OFF bit of SW_SOC_PD correct with the PCR bit (bit 0) of the GPC PGC Control Register (GPC_PGC_MIX_CTRL)?

 

We are currently reviewing the power saving implementation by comparing it with the Linux BSP source code.

In Linux source code "/drivers/soc/imx/gpcv2.c", it say that

/*
 * The PGC offset values in Reference Manual
 * (Rev. 1, 01/2018 and the older ones) GPC chapter's
 * GPC_PGC memory map are incorrect, below offset
 * values are from design RTL.
 */
#define IMX7_PGC_MIPI			16
#define IMX7_PGC_PCIE			17
#define IMX7_PGC_USB_HSIC		20

#define GPC_PGC_CTRL(n)			(0x800 + (n) * 0x40)
#define GPC_PGC_SR(n)			(GPC_PGC_CTRL(n) + 0xc)

And optee-os source "/core/drivers/pm/imx/suspend/psci-suspend-imx7.S"

#define MX7_SRC_GPR1	0x74
#define MX7_SRC_GPR2	0x78
#define GPC_PGC_C0	0x800
#define GPC_PGC_FM	0xa00

 

So it have difference between reference manual and Linux BSP source code.

PGC module nameReference Manual

Linux BSP code

PGC for A7 core00x303A_08000x303A_0800
PGC for A7 core10x303A_0840 
PGC for A7 SCU

0x303A_0880

 
PGC for fastmix/megamix

0x303A_0890(GPC_PGC_SCU_AUXSW?)

0x303A_08C0(GPC_PGC_MIX_CTRL?)

0x303A_0A00(GPC_PGC_FM)
PGC for MIPI PHY0x303A_0900

0x303A_0C00

BASE + (0x800 + (16) * 0x40)

PGC for PCIE_PHY0x303A_940

0x303A_0C40

BASE + (0x800 + (17) * 0x40)

PGC for USB HSIC PHY0x303A_0D00

0x303A_0D00

BASE + (0x800 + (20) * 0x40)

 

Q2. Which is correct address?

 

Best regards,

Ishii.

0 件の賞賛
返信
3 返答(返信)

441件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @takayuki_ishii!

Thank you for contacting NXP Support!

 

You have to refer to the Reference Manual.

 

Best Regards!

Chavira

0 件の賞賛
返信

402件の閲覧回数
takayuki_ishii
Contributor IV

Hello @Chavira 

 

Thank you for your answered.

 

> You have to refer to the Reference Manual.

I will write the source code by referring to the reference manual.

 

> Q1. Is the ON/OFF bit of SW_SOC_PD correct with the PCR bit (bit 0) of the GPC PGC Control Register (GPC_PGC_MIX_CTRL)?

What do you think of the answer to Q1?

 

I would appreciate your cooperation.

 

Best regards,

Ishii.

0 件の賞賛
返信

391件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @takayuki_ishii!

 

The GPC_PGC_MIX_CTRL should be PGC for fastmix/megamix and according to the diagram below.

 

Chavira_0-1723744134429.png

 

Best Regards!

Chavira

0 件の賞賛
返信