What USB pins are needed to use i.MX6UL as USB device only.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What USB pins are needed to use i.MX6UL as USB device only.

ソリューションへジャンプ
1,461件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about i.MX6UL USB.
They want to confirm what function should be assing to i.MX6UL pad to use i.MX6UL as USB device only.
Especially, whether OC and ID pin is needed or not.
I think both function pins are not needed with the following reason.
=====
For OC pin:
Over current detection is the function for USB host, so OC pin is not needed when use i.MX6UL as device.

For ID pin:
If ID is not assigned to any pins by IOMUX, ID will be floating.
In this case, i.MX6UL behave as USB device.
=====
Is my understanding correct?


Best Regards,
Satoshi Shimoda

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,246件の閲覧回数
art
NXP Employee
NXP Employee

Yes, your understanding is correct. Moreover, the USB controller should be configured in software so as it will operate in the Device mode only and will ignore OC and ID pins.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,247件の閲覧回数
art
NXP Employee
NXP Employee

Yes, your understanding is correct. Moreover, the USB controller should be configured in software so as it will operate in the Device mode only and will ignore OC and ID pins.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信