Weston sources?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Weston sources?

Jump to solution
2,662 Views
stephenminutill
Contributor II

I am working with the new 4.0.0 Linux BSP on i.MX6Q, with Qt and Wayland/Weston.  I need to make some customizations to Weston, but I can't find the sources.  The sources I'm looking for are those for the prebuilt Weston binaries in the package weston-imx-bin-3.0.35-4.0.0.tar.gz.  Can these sources be made available?

Labels (2)
Tags (1)
1 Solution
2,074 Views
lily_zhang
NXP Employee
NXP Employee
0 Kudos
Reply
4 Replies
2,075 Views
lily_zhang
NXP Employee
NXP Employee
0 Kudos
Reply
2,074 Views
aurelienbouin
Contributor IV

When fallowing the tuto you do not get the files needed : fb-backend.so and gal2d-backend.so

0 Kudos
Reply
2,074 Views
XiaoPong
NXP Employee
NXP Employee
0 Kudos
Reply
2,074 Views
AbhijitPotnis
Contributor I

I guess what stephenminutillo meant by sources is that he needed the sources for GAL2d and framebuffer backend implementation for weston. The files that generate fb-backend.so and gal2d-backend.so.

0 Kudos
Reply