WM8750 audio driver interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WM8750 audio driver interface

2,029件の閲覧回数
udayakumar
Contributor I

hi ,

we are using wm8750 audio codec ROUT2 as external speaker in our imx6q custom board, we couldn't able to control the volume through amixer command example: amixer sset Speaker 120

there is no effect in audio, which we hear look same. In default driver out3 is dapm_widget which is ON ,known by (cat /sys/class/sound/card0/device/HiFi/dapm_widget ) command.

Need to access ROUT2 volume in user space, so RIGHT_OUT2 dapm_widget need to be ON. Any suggestion to control ROUT2 volume in user space ? and how to ON  RIGHT_OUT2 dapm_widget ?

thanks,

uday#

ラベル(2)
0 件の賞賛
返信
1 返信

1,826件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi uday

one can try with alsamixer described on tutorial below

WM8960 audio codec 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信