WLAN,BT and GPS disable in Android Build

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

WLAN,BT and GPS disable in Android Build

跳至解决方案
1,825 次查看
anjojohn
Contributor IV

Hi all, 

i have a custom board with IMX6 based on sabresd. for reducing memory footprint , i would like to disable wlan, bt and gps module from building. Any help is appreciated

1 解答
1,721 次查看
igorpadykov
NXP Employee
NXP Employee

Hi anjo

one can look at Linux Manual included in Linux L4.14.98_2.0.0 Documentation

and disable appropriate drivers using section "Menu Configuration Options" Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,722 次查看
igorpadykov
NXP Employee
NXP Employee

Hi anjo

one can look at Linux Manual included in Linux L4.14.98_2.0.0 Documentation

and disable appropriate drivers using section "Menu Configuration Options" Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------