WLAN,BT and GPS disable in Android Build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WLAN,BT and GPS disable in Android Build

Jump to solution
1,830 Views
anjojohn
Contributor IV

Hi all, 

i have a custom board with IMX6 based on sabresd. for reducing memory footprint , i would like to disable wlan, bt and gps module from building. Any help is appreciated

1 Solution
1,726 Views
igorpadykov
NXP Employee
NXP Employee

Hi anjo

one can look at Linux Manual included in Linux L4.14.98_2.0.0 Documentation

and disable appropriate drivers using section "Menu Configuration Options" Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,727 Views
igorpadykov
NXP Employee
NXP Employee

Hi anjo

one can look at Linux Manual included in Linux L4.14.98_2.0.0 Documentation

and disable appropriate drivers using section "Menu Configuration Options" Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------