Voltage power up sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voltage power up sequence

1,282 Views
marijanvesligaj
Contributor I

What is the proper voltage power up sequence for MX6SoloX CPU?

As stated in datasheet, VDD_HIGH and VDD_SNVS can be powered up simuntaneously. What about other voltages then, especially core voltage and 3.3V IO.

Can everything be powered up at the same time?

Labels (1)
0 Kudos
Reply
1 Reply

1,075 Views
igorpadykov
NXP Employee
NXP Employee

Hi Marijan

everything can not be powered up at the same time,

datasheet also describes restrictions for VDD_ARM_IN and VDD_SOC_IN

in case external POR. In general recommended to follow i.MX6SX SDB deisgn

(with MMPF0100F6)

IMX6SOLOX-SABRESDB-DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply