Voltage power up sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Voltage power up sequence

1,298件の閲覧回数
marijanvesligaj
Contributor I

What is the proper voltage power up sequence for MX6SoloX CPU?

As stated in datasheet, VDD_HIGH and VDD_SNVS can be powered up simuntaneously. What about other voltages then, especially core voltage and 3.3V IO.

Can everything be powered up at the same time?

ラベル(1)
0 件の賞賛
返信
1 返信

1,091件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Marijan

everything can not be powered up at the same time,

datasheet also describes restrictions for VDD_ARM_IN and VDD_SOC_IN

in case external POR. In general recommended to follow i.MX6SX SDB deisgn

(with MMPF0100F6)

IMX6SOLOX-SABRESDB-DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信