Video Encoding capabilities of iMX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Video Encoding capabilities of iMX8M

6,928 Views
msingh1920
Contributor V

Hi Sir,

We are planning to use iMX8 M Quad and iMX8 M Plus for our product but have few questions regarding its video capabilities - 

1. What are the maximum video encoding capabilities of the iMX8M quad and plus? 

2. Is it possible to encode 4k60 with a hardware encoder or with any software encoder  ?

3. Can we use vpu for 4k60 Encoder?  what is the maximum limit of VPU for Encoding

4. Can we use vpu for 4k60 Decoder? what is the maximum limit of VPU for Decoding

 

Thanks,
Maneesh

0 Kudos
Reply
5 Replies

6,916 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maneesh

 

vpu capabilies can be found on below link

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

>2. Is it possible to encode 4k60 with a hardware encoder or with any software encoder ?

 

only with software encoder.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-mx8M-EVK-board-encoder-and-decoder/ta-...

 

Best regards
igor

0 Kudos
Reply

6,901 Views
msingh1920
Contributor V

Hi @igorpadykov 

Thanks for your reply. 

It cleared some of my doubts. But still, I have few doubts please help me to solve that. 

1. Is iMX8M Plus havs VCU800e  VPU ?

2. can it do jpeg 4k60 encoding?  

3. I am planning to use iMX8m Plus Board for SW Encoding at 4K 60fps and planning to try JPEG and technique. so is there any way I can utilize the VPU of iMX8m plus or it's not possible? 

 

2. Is there any steps or doc or anything is available for 4k60 encoding on imx8m plus ? 

 

3. do you have any idea what compression ratio we can achieve on iMX8m plus for JPEG encoding? 

 

Any suggestion or reply will be very helpful.

 

Thanks,
Maneesh

0 Kudos
Reply

6,897 Views
igorpadykov
NXP Employee
NXP Employee

1. yes

2. no

3. no way

 

Best regards
igor

0 Kudos
Reply

6,892 Views
msingh1920
Contributor V

Hi Sir @igorpadykov ,

Thanks a lot for your response. 


Please suggest how can I achieve 4k60 encoding with an iMX8 processor? 

Are there any reference documents or anything you can provide so that I can try to do 4k60 encoding? 

Also, on Hantro website => https://www.verisilicon.com/en/IPPortfolio/HantroVC8000E
it is mentioned that => 
Hantro VC8000E allows 4K encoding with a minimal silicon single-core solution that supports HEVC and H.264 video formats. HEVC / H264 multi-core solutions can also be used, which can reach 8K@30fps (dual-core).

so why it is not supported on the iMX8 processor? because iMX uses the same VPU. 

 

Thanks,
Maneesh

0 Kudos
Reply

6,881 Views
igorpadykov
NXP Employee
NXP Employee

>Are there any reference documents or anything you can provide so that I can try to do 4k60 encoding? 

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-mx8M-EVK-board-encoder-and-decoder/ta-...

 

Best regards
igor

 

 

0 Kudos
Reply