Viable Low Power Android Platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Viable Low Power Android Platform

Jump to solution
1,813 Views
deniscollis
Contributor V

Background.

I have IoT kiosk devices using Kinetis MCUs and FreeRTOS.  These are unattended solar powered devices using Kinetis MCU's running FreeRTOS and spend most of their lives in Ultra Low-Power mode, consuming only a few microamps.

I occasionally need to fire another 3rd party certified application, available only on Android, Linux or Windows. So I'm looking for the most energy-frugal and/or fastest-booting android platform.  The idea is to wake-up or boot the Android platform when needed, and invoke sleep-mode or shut it down when it is no longer needed.

Can this be achieved with an iMX MCU?

0 Kudos
Reply
1 Solution
1,803 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

For low power applications, you may be interested in taking a look at the following products:

 

i.MX 7ULP: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

i.MX 6ULL: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

Hope it helps!

 

BR,

Ivan.

View solution in original post

0 Kudos
Reply
1 Reply
1,804 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

For low power applications, you may be interested in taking a look at the following products:

 

i.MX 7ULP: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

i.MX 6ULL: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

Hope it helps!

 

BR,

Ivan.

0 Kudos
Reply