Viable Low Power Android Platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Viable Low Power Android Platform

ソリューションへジャンプ
1,807件の閲覧回数
deniscollis
Contributor V

Background.

I have IoT kiosk devices using Kinetis MCUs and FreeRTOS.  These are unattended solar powered devices using Kinetis MCU's running FreeRTOS and spend most of their lives in Ultra Low-Power mode, consuming only a few microamps.

I occasionally need to fire another 3rd party certified application, available only on Android, Linux or Windows. So I'm looking for the most energy-frugal and/or fastest-booting android platform.  The idea is to wake-up or boot the Android platform when needed, and invoke sleep-mode or shut it down when it is no longer needed.

Can this be achieved with an iMX MCU?

0 件の賞賛
返信
1 解決策
1,797件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

For low power applications, you may be interested in taking a look at the following products:

 

i.MX 7ULP: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

i.MX 6ULL: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

Hope it helps!

 

BR,

Ivan.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,798件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

For low power applications, you may be interested in taking a look at the following products:

 

i.MX 7ULP: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

i.MX 6ULL: https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

Hope it helps!

 

BR,

Ivan.

0 件の賞賛
返信