VPU source code for iMX.6 and Windows Embedded Compact 2013

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU source code for iMX.6 and Windows Embedded Compact 2013

ソリューションへジャンプ
4,032件の閲覧回数
misbahkhan
Contributor II

Hello All,

We need the source code for building VPU lib for WEC2013 Without which we cannot have "vpu_mx6q_fsl_v4.lib" for WEC2013

and there by VPU will never be working for WEC2013

Please help out to resolve this issue.

If you cannot give the source at least give us the "vpu_mx6q_fsl_v4.lib" binary compiled for WEC2013 "Thumb-2"

Hoping for a response from your side.

Thanks,

Misbah

1 解決策
2,863件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

Can you check with Adeneo for it. Adeneo is our 3rd party to provide i.mx6 WEC2013 BSP.

元の投稿で解決策を見る

3 返答(返信)
2,864件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

Can you check with Adeneo for it. Adeneo is our 3rd party to provide i.mx6 WEC2013 BSP.

2,863件の閲覧回数
pawel
Contributor II

I contacted Adeneo and the said that there is no plan to release VPU for WEC2013, which lead to a question, what to do then? I think there is a few vendors and many companies which are wiling to use i.MX6 VPU for their Windows Embedded based projects.

0 件の賞賛
返信
2,863件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

If that, you can contact with Freescale Sales/Marketing team for it.

Maybe they can find a right provider.