Hello,
I want to build a simple C file, where I try to initialize the VPU on my imx6Q.
The sysroot has been obtained via Yocto and bitbake (latest dora branch), poky toolchain version @ 1.5.3.
My code is:
----------------------------------
#include <vpu_io.h>
#include <vpu_lib.h>
void func(void)
{
int ret = 0, i;
// Init VPU
if(vpu_Init (NULL) < 0)
{
printf(">> failed to call vpu_Init()\n");
ret = -1;
}
}
-----------------------------------
full GCC command:
----------------------------------
arm-poky-linux-gnueabi-g++ -march=armv7-a -mthumb-interwork -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9 --sysroot=/home/raziel/Programming/SDKs/poky/1.5.3/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi -DHAVE_CONFIG_H -I. -I. -I.. --sysroot=/home/raziel/Programming/Workspace/Yocto/build/tmp/sysroots/nitrogen6x -I/home/raziel/Programming/Workspace/Yocto/build/tmp/sysroots/nitrogen6x/usr/include -I/home/raziel/Programming/Workspace/Yocto/build/tmp/sysroots/nitrogen6x/usr/src/kernel/include -fpermissive -g -O0 --sysroot=/home/raziel/Programming/Workspace/Yocto/build/tmp/sysroots/nitrogen6x -MT video_test.o -MD -MP -MF .deps/video_test.Tpo -c -o video_test.o video_test.cpp
arm-poky-linux-gnueabi-libtool --tag=CXX --mode=link arm-poky-linux-gnueabi-g++ -march=armv7-a -mthumb-interwork -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9 --sysroot=/home/raziel/Programming/SDKs/poky/1.5.3/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi -I/home/raziel/Programming/Workspace/Yocto/build/tmp/sysroots/nitrogen6x/usr/include -I/home/raziel/Programming/Workspace/Yocto/build/tmp/sysroots/nitrogen6x/usr/src/kernel/include -fpermissive -g -O0 --sysroot=/home/raziel/Programming/Workspace/Yocto/build/tmp/sysroots/nitrogen6x -lvpu --sysroot=/home/raziel/Programming/Workspace/Yocto/build/tmp/sysroots/nitrogen6x -o video_test
--------------------------------------
I am specifying -lvpu as an argument to GCC, except that libtool complains:
undefined reference to 'vpu_Init(void*)'
I fail to see what the issue is, given the fact that GCC finds the library just fine.
Manually specifying the full path to libvpu.a or libvpu.so from the Yocto sysroot dir lead to the same result, undefined reference.
What am I doing wrong?
解決済! 解決策の投稿を見る。
Wrap the #include directive of vpu library headers inside extern "C".
new code:
extern "C"
{
#include <vpu_io.h>
#include <vpu_lib.h>
}
void func(void)
{
int ret = 0, i;
// Init VPU
if(vpu_Init (NULL) < 0)
{
printf(">> failed to call vpu_Init()\n");
ret = -1;
}
}
this is because vpu library code is C compliant and I was using a C++ compiler to include a C generated library.
Wrap the #include directive of vpu library headers inside extern "C".
new code:
extern "C"
{
#include <vpu_io.h>
#include <vpu_lib.h>
}
void func(void)
{
int ret = 0, i;
// Init VPU
if(vpu_Init (NULL) < 0)
{
printf(">> failed to call vpu_Init()\n");
ret = -1;
}
}
this is because vpu library code is C compliant and I was using a C++ compiler to include a C generated library.
Hi,
Thank you for sharing your solution. It is very appreciated.
Best Regards,
Alejandro