CTS android.holo test case not running

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CTS android.holo test case not running

2,647 Views
jblack547
Contributor II

When we run our 4.4_r1 test this test case does not run. Also, there is another holo test, android.host.holo and it doesn't even show up in the results.

The Freescale CTS test results do not mention this test case.

Anyone else having this experience?

Test Package     Passed    Failed   Timed Out    Not Executed    Total Tests

android.holo       0               0          0                   0                        0

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,183 Views
jblack547
Contributor II

This test is officially removed from CTS for the time being. It will be put back at a future date. I removed it from the CTS.xml file to prevent the entry from messing up our test runs. We are using proprietary hardware based on SabreSD.

0 Kudos
Reply

2,183 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi James,

Which board are you using now?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,183 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi James,

Does it work now?

Best Regards

Dan

0 Kudos
Reply