VPU encode on i.MX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,205件の閲覧回数
xu_ji1
Contributor V

Hello,

Does i.MX8 VPU encode support V4L2_Y12 format input source to make avi or mp4?

use unit_test/V4L2_VPU/ or GSTL VPU used demo

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
5,826件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, vpu supports yuv420 only

元の投稿で解決策を見る

0 件の賞賛
返信
14 返答(返信)
5,826件の閲覧回数
xu_ji1
Contributor V

is there any voice?

0 件の賞賛
返信
5,826件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

sorry for my delay, do you mean raw 12 bits data input, right? current vpu doesn't support this format, and imx8x uses ISI to capture video and can support raw data, you can convert this in the ISI first, then send it to the vpu

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

Hello,

How about Raw 16 bits,VPU support or not?

How does IPU convert it?any API in IPU side?

0 件の賞賛
返信
5,826件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

vpu doesn't support raw data, but ISI does, i.mx8x uses ISI to convert data, for detailed information about ISI, pls refer to the imx8x reference manual, which has detailed information, and also check Figure 1-1. i.MX 8QuadXPlus/i.MX 8DualXPlus Simplified Block Diagram, you can find the data flow from camera

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

Hello,

please give the answer

0 件の賞賛
返信
5,827件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, vpu supports yuv420 only

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

Which image format does VPU support? I see from unit_test/V4L2_VPU/mxc_v4l2_vpu_enc VPU only support NV12 now,is it right?

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

Hello,

How about my question?

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

hi,

Any one can help this question?

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

is any one can help my question?

0 件の賞賛
返信
5,826件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what imx8 products  do you mean?i.mx8MQ, imx8X or iMX8MM?

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

Hello,

 

How about my question?

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

hello Joan,

How about my question? 

0 件の賞賛
返信
5,826件の閲覧回数
xu_ji1
Contributor V

it is imx8X

0 件の賞賛
返信