VPU Encoder clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU Encoder clarification

1,448件の閲覧回数
itzikperetz
Contributor I

I have some other questions:

1. Can you explain me what is the sliceMode parameter in the encoder?

2. What the differences between the available modes? Is sliceSize related to NALU Size?

3. I saw that the encoder only supports Base profile, but i didn't see any limitation regarding to set H264 level. Can you explain me how to set the level for the encoder?

Thanks,

Itzik

ラベル(2)
0 件の賞賛
返信
1 返信

1,360件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  “A slice is a spatially distinct region of a frame that is encoded separately from

any other region in the same frame. In that standard, instead of I-frames, P-frames,

and B-frames, there are I-slices, P-slices, and B-slices”.

  As for VPU slice mode details, please take a look at section 3.2.2.10 (EncSliceMode)

of “i.MX_6_VPU_Application_Programming_Interface_Linux_Reference_Manual.pdf”.

  As for profile and level setting, please refer to section 3.2.2.4 (EncHeaderParam).

https://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_iMX6QDLS_BUNDLE&appType=license&loc...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信