VPU Decoding core clock setting in i.MX515

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU Decoding core clock setting in i.MX515

ソリューションへジャンプ
3,713件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I plan to use VPU of i.MX515.

So I read MCIMX51RM Rev. 1 2/2010 but I can't find how to set a decoding core clock domain (cclk).

I know the decoding core clock comes from the CCM module because I found the following description in section 61.2.1.

All VPU input clock and reset sources come from the i.MX51 CCM module. The VPU does not do clock gating internally.

However, I can't understand which register do I set.

Q1.

Could you specify which register do I set to use VPU ?

Q2.

According to the section 61.4.2 of RM, the decoding core clock domain's frequency can scale done through the VPU API.

I can't find the API in L2.6.35_10.11.01_ER_docs/doc/mx5/i.MX5x_Linux_VPU_API.pdf.

Which VPU API can set the core clock frequency ?

Ko-hey

ラベル(2)
0 件の賞賛
返信
1 解決策
3,554件の閲覧回数
art
NXP Employee
NXP Employee

Q. VPU_AXI_CLK_ROOT will be enable when user set CG3 field to "11". Am I correct ?

A. Yes.

Q. VPU_RCLK_ROOT will be enable when user set CG4 field to "11". Am I correct ?

A. Yes.

Q. Which VPU API can set the core clock frequency ?

A. Actually, there is some inaccuracy in the manual. In fact, the decoding clock is derived from the AXI clock and has the equal frequency (typically, 166MHz). There is no separate mechanism to change the decoding clock frequency.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,554件の閲覧回数
ko-hey
Senior Contributor II

Could someone follow and answer the following question ?

I checked MCIMX51RM Rev. 1 2/2010 onemore time and found the CCGR5 Register can enable the VPU clock.

CG3 field can enable "vpu clocks" and CG4 field can enable "vpu reference clock".

 

On the other hand, according to the Figure 7-41 and Figure 7-44 of RM, the clock relate to VPU is as follow.

VPU_AXI_CLK_ROOT

VPU_RCLK_ROOT

Q1-1.

VPU_AXI_CLK_ROOT will be enable when user set CG3 field to "11".

Am I correct ?

 

Q1-2.

VPU_RCLK_ROOT will be enable when user set CG4 field to "11".

Am I correct ?

Q2 

According to the section 61.4.2 of RM, the decoding core clock domain's frequency can scale done through the VPU API.

I can't find the API in L2.6.35_10.11.01_ER_docs/doc/mx5/i.MX5x_Linux_VPU_API.pdf.

 

Which VPU API can set the core clock frequency ?

 

Ko-hey

3,555件の閲覧回数
art
NXP Employee
NXP Employee

Q. VPU_AXI_CLK_ROOT will be enable when user set CG3 field to "11". Am I correct ?

A. Yes.

Q. VPU_RCLK_ROOT will be enable when user set CG4 field to "11". Am I correct ?

A. Yes.

Q. Which VPU API can set the core clock frequency ?

A. Actually, there is some inaccuracy in the manual. In fact, the decoding clock is derived from the AXI clock and has the equal frequency (typically, 166MHz). There is no separate mechanism to change the decoding clock frequency.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,554件の閲覧回数
ko-hey
Senior Contributor II

So would you revise the manual ?

Ko-hey

0 件の賞賛
返信
3,554件の閲覧回数
art
NXP Employee
NXP Employee

Actually, i.MX51 is quite obsolete part, so, I don't think that someone will ever revise its documentation.

Artur

0 件の賞賛
返信
3,554件の閲覧回数
ko-hey
Senior Contributor II

Okay, thanks.

Ko-hey

0 件の賞賛
返信