V4L2_MEMORY_USERPTR support in MIPI camera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

V4L2_MEMORY_USERPTR support in MIPI camera

ソリューションへジャンプ
2,776件の閲覧回数
titusstalin
Contributor V

Dear All,

iMX MIPI camera supports V4L2_MEMORY_USERPTR method ?

Currently I'm using V4L2_MEMORY_MMAP method, want to use USERPTR.

Can you please reply to this question ?

Regards,

Titus S.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,153件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,


  the following may be helpful

https://community.nxp.com/thread/359579 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,154件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,


  the following may be helpful

https://community.nxp.com/thread/359579 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信
2,153件の閲覧回数
titusstalin
Contributor V

Sounds good.

Thanks for the reply.

0 件の賞賛
返信