Using uuu to load imx8mq eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using uuu to load imx8mq eMMC

4,591 Views
tuban
Contributor I

I am working with a custom board using an imx8mq Variscite SOM with eMMC only (no SD) and have successfully used uuu to load linux images using uuu, but am having difficulty loading android 10. I see posts for both 'uuu android.zip' and 'uuu-android-mx8mm-evk-emmc.lst', but I do not know how to create android.zip and cannot find the .lst script which I may be able to modify for my situation.

Any help would be appreciated.

--tnx

--tom

0 Kudos
Reply
3 Replies

4,526 Views
tuban
Contributor I

My Arrow field engineer helped me discover the uuu_imx_android_flash.sh script in the android build output directory.

I've been messing with it and have made some progress, but now it appears that the eMMC load hangs. I made a couple of changes to the script to accept var-dart et al in order to align it with my build output. I also added -v -V to the uuu args.

Here is the generated uuu.lst file:

uuu_version 1.3.102
SDP: boot -f u-boot-imx8mq-var-dart-uuu.imx
SDPU: delay 1000
SDPU: write -f u-boot-imx8mq-var-dart-uuu.imx -offset 0x57c00
SDPU: jump
SDPV: delay 1000
SDPV: write -f u-boot-imx8mq-var-dart-uuu.imx -skipspl
SDPV: jump
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev 0
FB: ucmd mmc dev 0
FB: ucmd mmc dev 0 0
FB: ucmd mmc erase 0x2000 0x8
FB: ucmd mmc partconf 0 1 1 1
FB: flash bootloader0 u-boot-imx8mq-var-dart.imx
FB: flash gpt partition-table.img
FB: ucmd setenv fastboot_dev sata
FB: ucmd setenv fastboot_dev mmc
FB: flash dtbo_a dtbo-imx8mq-var-dart-sd-hdmi.img
FB: flash boot_a boot.img
FB: flash system_a system.img
FB: flash vendor_a vendor.img
FB: flash product_a product.img
FB: flash vbmeta_a vbmeta-imx8mq-var-dart-sd-hdmi.img
FB[-t 600000]: erase misc
FB[-t 600000]: erase presistdata
FB[-t 600000]: erase fbmisc
FB: set_active a
FB[-t 600000]: erase userdata
FB: done

Here is my script call and output:

~/var_imx-android-10.0.0_1.0.0/android_build/out/target/product/dart_mx8mq$ sudo ./uuu_imx_android_flash.sh -f imx8mq -a -e -t emmc -u var-dart -d var-dart-sd-hdmi -p var-dart
This script is validated with uuu 1.3.102 version, please align with this version.
dtbo is supported
dual slot is supported
generate lines to flash u-boot-imx8mq-var-dart.imx to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx8mq-var-dart-sd-hdmi.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash product.img to the partition of product_a
generate lines to flash vbmeta-imx8mq-var-dart-sd-hdmi.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.154-0-g47ddef5

Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
Wait for Known USB Device Appear...
New USB Device Attached at 1:21
1:21>Start Cmd:SDP: boot -f u-boot-imx8mq-var-dart-uuu.imx
6400%1:21>Okay (2.68s)
^C (I interrupted here after waiting for a while without any signs of progress)

Here is the device console output:

U-Boot SPL 2019.04-41456-g4de18fd2b7 (Jul 21 2020 - 07:55:47 -0500)
PMIC: PFUZE100 ID=0x10

0 Kudos
Reply

4,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tom

for building image one can look at sect.3 Building the Android platform for i.MX Android User’s Guide

Android OS for i.MX Applications Processors | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,526 Views
tuban
Contributor I

Thanks for helping on this Igor. Let me explain more of the details. I am able to build the android image set successfully. I have even been able to load built images onto the variscite demo board, which has SD. My problem is loading our custom board which only has eMMC. I am running under Ubuntu, not windows. I have successfully used the uuu tool under Ubuntu to load the linux build onto eMMC (via USB). I see references to being able to either use 'uuu android.zip' to load eMMC via USB and 'uuu uuu-android-mx8mm-evk-emmc.lst'. I believe that if I can find a .lst file example, I can tailor it to our system. Or, if I knew what files to zip together, that may work too. I just don't see instructions for either of these in the documentation or other forum questions. Do I really have to run Windows to do this?

0 Kudos
Reply