Pre-Requisite for running Kmemleak Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pre-Requisite for running Kmemleak Tool

1,606 次查看
pavithrapadmana
Contributor I

Hi,

I am using imx6dq device, running with AOSP 6, kernel - 4.1.15  and booting the device with sd card spec of 8GB.

I tried to run the Kmemleak tool in the target device. But my device is getting into error state and reboot is happening.

I checked the log and i found the below line

mmcblk1: p4 size 12689664 extends beyond EOD, truncated

mmcblk1 is sd card and p4 is data partition.

Will this issue cause the device to reboot or let into hang state??

Is there any Pre-requisite such as minimum memory requirement to run the Kmemleak tool?

Thanks in advance..

标签 (1)
0 项奖励
回复
1 回复

1,571 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Pavithra P,

As far as a know there is not a minimum memory requirement to run Kmemleak.

There is some information on the Android Documentation on how this tool works.

https://android.googlesource.com/kernel/common/+/a7827a2a60218b25f222b54f77ed38f57aebe08b/Documentat...

From the error shown, it looks like there is a problem with the partitions so maybe that’s what’s causing the error and not the lack of memory.

I would recommend looking into AOSP forums reporting similar errors to try finding the root cause.

I hope this helps!

Regards,

0 项奖励
回复