Using two pn7150 on the same imx6sx board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using two pn7150 on the same imx6sx board

Jump to solution
1,954 Views
longh
Contributor III

Hi all,

     Because of the application needs, we need to use two pn7150 on the same imx6sx board. Can this be achieved through libnfc NCI?Or other implementation methods.

Labels (2)
0 Kudos
Reply
1 Solution
1,874 Views
igorpadykov
NXP Employee
NXP Employee

Hi long

one can look at

NFC in Android Lollipop 5.0.0 

https://community.nxp.com/docs/DOC-343207 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,875 Views
igorpadykov
NXP Employee
NXP Employee

Hi long

one can look at

NFC in Android Lollipop 5.0.0 

https://community.nxp.com/docs/DOC-343207 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------