Using two pn7150 on the same imx6sx board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using two pn7150 on the same imx6sx board

跳至解决方案
1,224 次查看
longh
Contributor III

Hi all,

     Because of the application needs, we need to use two pn7150 on the same imx6sx board. Can this be achieved through libnfc NCI?Or other implementation methods.

标签 (2)
0 项奖励
回复
1 解答
1,144 次查看
igorpadykov
NXP Employee
NXP Employee

Hi long

one can look at

NFC in Android Lollipop 5.0.0 

https://community.nxp.com/docs/DOC-343207 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,145 次查看
igorpadykov
NXP Employee
NXP Employee

Hi long

one can look at

NFC in Android Lollipop 5.0.0 

https://community.nxp.com/docs/DOC-343207 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------