Using the __libc_init_array() in C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using the __libc_init_array() in C

2,021 次查看
andréluis
Contributor II

Hi, i'm working with a RT1060 and i compile a program using the 4diac with the runtime Forte. The question is the Forte need the __libc_init_array() to run. And need to run in freeRtos with Lwip because the architecture need to be in Freertos. But Lwip work with C. Can i use this function (__libc_init_array()) in C to run the Forte? 

0 项奖励
回复
2 回复数

1,996 次查看
andréluis
Contributor II

Hi Bio_TICFSL, how can i put this function before the main?

0 项奖励
回复

2,001 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes you can use it but, This serves calling constructors and other library initialization which is necessary before calling main. There is a good description about this as well on :

https://stackoverflow.com/questions/15265295/understanding-the-libc-init-array

Regards

0 项奖励
回复