Using the CSI inputs on IMX6DQCEC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the CSI inputs on IMX6DQCEC

ソリューションへジャンプ
2,750件の閲覧回数
davidbrooks
Contributor I

Hi,

I'd like to drive the CSI inputs from a DSI (Display Serial Interface: in effect, serialized BT.565) signal source, but from what I can see, the serial camera inputs only accept proprietary signal standards such as MIPI. Will DSI work, or alternatively, are there any other public serial data standards which CSI can accept?

Regards & TIA

0 件の賞賛
返信
1 解決策
2,444件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,David,

      There are 3 kinds of camera interface:

(1)CS0 port (parallel interface)

CSI0.png

(2)CS1 port (parallel interface)

CSI1.png

(3)MIPI port (serial interface)
MIPI.png

     In addition, DSI port is display output . Not camera signal input .

Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,445件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,David,

      There are 3 kinds of camera interface:

(1)CS0 port (parallel interface)

CSI0.png

(2)CS1 port (parallel interface)

CSI1.png

(3)MIPI port (serial interface)
MIPI.png

     In addition, DSI port is display output . Not camera signal input .

Regards,

Weidong

0 件の賞賛
返信
2,444件の閲覧回数
davidbrooks
Contributor I

Many thanks, Weidong.

Those picture make it all clear.

Regards

0 件の賞賛
返信