Using the ADC of MIMXRT 1160-EVK to sample an external signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using the ADC of MIMXRT 1160-EVK to sample an external signal

跳至解决方案
1,051 次查看
HousseinKanso
Contributor I

Hello, 

I am using the MIMXRT 1160-EVK controller. 

I want to use its internal ADC to sample an external signal coming from a clamp-meter (current data coming from one of the phase of a permanent-magnet synchronous motor). The signal will be transformed first from single-ended mode to differential mode (twisted-pair) before being fed to the controller. So, I need to use the differential signaling mode. The ADC should start doing the conversions after receiving some external signal when the motor starts rotating (most probably coming from FreeMaster lite) and will stop using the same method. The purpose is to be able to record this current data, and then write it into a log file. I looked into many lpadc examples, but none of them is similar to what I am trying to do. I am still new to the embedded field, so any help/advice would be appreciated.

 

标签 (1)
0 项奖励
回复
1 解答
1,038 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend using the k64 this has an ADC differential and you can modify the example SDK to see how works.

Maybe this post help you to understand the ADC functionality. Understanding ADC specifications - NXP Community

Best regards,
Pavel

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,039 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend using the k64 this has an ADC differential and you can modify the example SDK to see how works.

Maybe this post help you to understand the ADC functionality. Understanding ADC specifications - NXP Community

Best regards,
Pavel

0 项奖励
回复