Hello,
I am using the MIMXRT 1160-EVK controller.
I want to use its internal ADC to sample an external signal coming from a clamp-meter (current data coming from one of the phase of a permanent-magnet synchronous motor). The signal will be transformed first from single-ended mode to differential mode (twisted-pair) before being fed to the controller. So, I need to use the differential signaling mode. The ADC should start doing the conversions after receiving some external signal when the motor starts rotating (most probably coming from FreeMaster lite) and will stop using the same method. The purpose is to be able to record this current data, and then write it into a log file. I looked into many lpadc examples, but none of them is similar to what I am trying to do. I am still new to the embedded field, so any help/advice would be appreciated.