Using qt in I.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using qt in I.MX6UL

Jump to solution
2,955 Views
JHY
Contributor IV

I.MX6UL has no accelerator for 2D/3D.

Does it mean that I.MX6UL can't use QT applications at all?

Labels (1)
Tags (1)
1 Solution
2,503 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

in general it can use as discussed on meta-fsl-arm mailing list:

Freescale OpenEmbedded/Yocto Layers discussion list ()

however it is not supported in official bsp, refer to attached Release Notes p.8.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,504 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

in general it can use as discussed on meta-fsl-arm mailing list:

Freescale OpenEmbedded/Yocto Layers discussion list ()

however it is not supported in official bsp, refer to attached Release Notes p.8.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------