Using mpDemon with i.MX53 QSB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using mpDemon with i.MX53 QSB

1,382 Views
AlanLevy
Contributor I
Has anybody succeeded in getting an mpDemon to work with a QSB? I've got the ARM personality module connected up to the board, I've configured the firmware to talk to an i.MX51 (it doesn't know about i.MX53) and I've told OCDCommander that it's talking to an i.MX53. Whatever I try, OCDCommander reports that the cable isn't connected.
0 Kudos
Reply
2 Replies

1,327 Views
AlanLevy
Contributor I
No - our MpDemon turned out to be faulty. I've sent it back to Macraigor for repair but they have been appallingly slow to fix it. They're telling me it's because of problems with component availability.
0 Kudos
Reply

1,327 Views
DougMartens
Contributor II

Alan,

 

Have you had any luck with getting the Macraigor tools to talk to an iMX53 board?  Our production board will be complete sometime this week and I may need a JTAG tool.  This is the tool that I am the most familar with and I'm leaning towards it.

0 Kudos
Reply