Using mpDemon with i.MX53 QSB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using mpDemon with i.MX53 QSB

1,365件の閲覧回数
AlanLevy
Contributor I
Has anybody succeeded in getting an mpDemon to work with a QSB? I've got the ARM personality module connected up to the board, I've configured the firmware to talk to an i.MX51 (it doesn't know about i.MX53) and I've told OCDCommander that it's talking to an i.MX53. Whatever I try, OCDCommander reports that the cable isn't connected.
0 件の賞賛
返信
2 返答(返信)

1,310件の閲覧回数
AlanLevy
Contributor I
No - our MpDemon turned out to be faulty. I've sent it back to Macraigor for repair but they have been appallingly slow to fix it. They're telling me it's because of problems with component availability.
0 件の賞賛
返信

1,310件の閲覧回数
DougMartens
Contributor II

Alan,

 

Have you had any luck with getting the Macraigor tools to talk to an iMX53 board?  Our production board will be complete sometime this week and I may need a JTAG tool.  This is the tool that I am the most familar with and I'm leaning towards it.

0 件の賞賛
返信