Using /dev/caam_kb to generate key blobs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using /dev/caam_kb to generate key blobs

2,984 Views
terateller
Contributor II

Hi All,

The Yocto build has a /dev/caam_kb when CAAM is enabled. Does anyone know or refer me to some documentation on how to generate a key blob(using OTPMK?) using this ioctl device interface?

Is there some examples or documentation? How can CAAM be called to make a key blob using OTPMK? 

Thanks,

Tera

Tags (1)
0 Kudos
Reply
2 Replies

2,606 Views
terateller
Contributor II

Dear All,

I chanced upon the dek_blob tool in connection with HABv4.

So from what I read, using this tool one can generate use a DEK (encryption key) and encrypt data. In case of HAB, using this tool, we can encrypt our uboot image, isn't it?

Here is how the command can be used:

dek_blob <DEK address> <Output Address> <Key Size in Bits>

Here what is the DEK Address? Also, does this command per default use the OTPMK , i.e the master key bound to each chip burned in silicon?

Please throw light. 

Thanks a lot.

0 Kudos
Reply

2,606 Views
joanxie
NXP TechSupport
NXP TechSupport

you need to use the signed U-boot. pls refer to the document as below:

https://community.nxp.com/docs/DOC-330622 

0 Kudos
Reply