Using a custom GStreamer plugin on imx233

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using a custom GStreamer plugin on imx233

1,344件の閲覧回数
TB
Contributor I

Hi, has anyone managed to create a gstreamer plugin using the template kit and built it so that it works on a freescale board (specifically the imx233)? My plugin builds fine for windows but won't come up on the board with gst-inspect saying:

(gst-inspect-0.10:714): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libspadecoder.so': /usr/lib/gstreamer-0.10/libspadecoder.so: cannot open shared object file: No such file or directory

(And yes, the files mentioned there do exist at those paths).

I've tried changing a couple of things having looked at the freescale plugin package and how that builds, but I'm not great with how the configure/make files operate and so far nothing I've tried has changed the above message.

タグ(2)
0 件の賞賛
返信
0 返答(返信)