Using USB device without VDD5V on imX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using USB device without VDD5V on imX28

Jump to solution
1,975 Views
MartinHo
Contributor IV

I would like to use the USB OTG Port in device only mode without having VDD5V present. I have seen that there is a patch for Linux L2.6.35_1.1.0 (USB Device not work when VDD5V is not attached during boot (iMX28)).

Is there a similar patch for windows CE 6.0?

best regards

martin

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
1,821 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

I am afraid there are no such patches for WinCE60.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,822 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

I am afraid there are no such patches for WinCE60.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply