Using USB device without VDD5V on imX28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using USB device without VDD5V on imX28

ソリューションへジャンプ
1,968件の閲覧回数
MartinHo
Contributor IV

I would like to use the USB OTG Port in device only mode without having VDD5V present. I have seen that there is a patch for Linux L2.6.35_1.1.0 (USB Device not work when VDD5V is not attached during boot (iMX28)).

Is there a similar patch for windows CE 6.0?

best regards

martin

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,814件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Martin

I am afraid there are no such patches for WinCE60.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,815件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Martin

I am afraid there are no such patches for WinCE60.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信