Using Segger j-link with IMX8M plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Segger j-link with IMX8M plus

ソリューションへジャンプ
6,242件の閲覧回数
niklasbergdahl
Contributor I

Are there any device-files to use with segger when debugging the M7 of an IMX8M Plus?
I'm trying to debug the M7 of an i.MX 8M Plus EVK, but run into trouble when trying to connect and reset.

タグ(1)
0 件の賞賛
返信
1 解決策
6,237件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

 

one can try IAR and SEGGER tool patch for i.MX8M Plus devices

and SDK_EVK-MIMX8MP available on

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,735件の閲覧回数
illy777
Contributor III

Hi there, is there an updated solution, because this doesn't work properly or I'm doing something wrong.

 

I'm on Windows 10, using the J-Flash 7.86 version: There is no support for the MIMX8MPRM devices.. I alredy did what the readme of the file above told and also tried downloading the instructions of the J-Link page - debugger starter kit. 

Therefore I put the files in following order in the %APPDATA%/../SEGGER-folder:

illy777_0-1680074546263.png

I also changed the .xml file:

illy777_1-1680074600551.png

It would help me a lot if anyone know further details or can reach me a hand!

 

Thank you!

 

 

 

 

0 件の賞賛
返信
6,238件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

 

one can try IAR and SEGGER tool patch for i.MX8M Plus devices

and SDK_EVK-MIMX8MP available on

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 件の賞賛
返信