Using Segger JLinkExe to halt / resume IMX6ULL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using Segger JLinkExe to halt / resume IMX6ULL?

跳至解决方案
3,473 次查看
djregan
Contributor III

Hello,

I am using the IMX6ULL and was curious if anyone else has observed this scenario?...

1. Attach Segger JLink Plus to IMX6ULL JTAG interface

2. Power up IMX6ULL

3. Allow 1st stage program loading efforts to stream u-Boot from SPI NOR into DDR (or other start-up media if not using SPI NOR)

4. Allow IMX6ULL to begin executing the existing SPI NOR originated u-boot from DDR (or other start-up media if not using SPI NOR)

5. Use JLinkExe to issue 'h' - halt command

6. Use JLinkExe command 'loadbin' with a new u-boot.bin image beginning from the 1st u-boot.bin instruction address through the end of the new u-boot image

7. Use JLinkExe to issue 'setPC' - set Program Counter command to set the program counter to the 1st instruction in the new u-boot.bin file, which was loaded via JTAG.

8. Use JlinkExe to issue 'g' - Go command

9. Monitor IMX6ULL debug UART traffic to observe the execution response of u-boot

....what I'm seeing is -> the u-boot 'ver' command hints that the actual u-boot version being run following the above sequence is the older u-boot image. So... to me it hints the target is re-running 1st stage program loading efforts and re-streaming the old u-boot.bin image into DDR after step '8.' in the sequence above.

And... if this theory is correct - >1st stage program loading is re-run after step '8.' above?... Is there a way to sequence IMX6ULL execution control such that a new u-boot.bin image can be streamed into DDR over JTAG without subsequently watching it get blown away by a re-execution of 1st stage program re-re-loading efforts?

Thanks much in advance!

Regards,

--DJ Regan

标签 (1)
标记 (2)
1 解答
3,189 次查看
djregan
Contributor III

Plan B... I was able to control 'which?' u-boot image by placing IMX6ULL in 'Serial Download' mode (via boot mode select pins)... then use Segger JLinkExe to control which version of u-boot is in DDR. That works. Above concerns are now a non-issue.

Please consider my question as 'Answered'. :smileyhappy:

Thanks much...

--DJ Regan

在原帖中查看解决方案

2 回复数
3,189 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  U-boot generally is not position independent, therefore this is not good idea to load

simultaneously "old" and "new" U-boots.

Regards,

Yuri.

3,190 次查看
djregan
Contributor III

Plan B... I was able to control 'which?' u-boot image by placing IMX6ULL in 'Serial Download' mode (via boot mode select pins)... then use Segger JLinkExe to control which version of u-boot is in DDR. That works. Above concerns are now a non-issue.

Please consider my question as 'Answered'. :smileyhappy:

Thanks much...

--DJ Regan