Using SAI2 root clock for SAI1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using SAI2 root clock for SAI1

1,630 Views
ovalentin
Contributor I

Hello,

I would need to have different sample rates for SAI1_RX and SAI1_TX, so I am trying to use SAI2 clock for one of them, as proposed in I2Sx_xCR2/MSEL.

Unfortunately, this leads to a silent clock and no transfer.

The documentation states (Ref Manual p4327) "Depending on the device, some Master Clock options might not be available. See the chip-specific information for the availability and chip-specific meaning of each option."

So my question is twofold:

- Is it legal to attempt to use SAI2 root clock for one of SAI1 streams ?

- Where may I find the "chip-specific information" for i.MX7D?

Best regards,

Olivier

Labels (2)
0 Kudos
Reply
1 Reply

1,499 Views
igorpadykov
NXP Employee
NXP Employee

Hi Olivier

MSEL can select only one clock, two options are not available,

may be useful link

MX7D how to obtain 2 different SAI MCLKs 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply