Using PWM outputs as clock source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using PWM outputs as clock source

ソリューションへジャンプ
1,901件の閲覧回数
atillametetured
Contributor V


Greetings,

We are designing a custom HW using iMX6Q and one of our peripheral devices needs a clock source of 32.768 kHz. Can we supply this through one of the PWM I/O on iMX? If not what port can I use to supply a peripheral with a clock at this frequency?

Regards,

Mete

ラベル(2)
タグ(5)
0 件の賞賛
返信
1 解決策
1,652件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The following may help  i.MX6S CLKO1 does not output 32kHz.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,653件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The following may help  i.MX6S CLKO1 does not output 32kHz.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------