Using PWM outputs as clock source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using PWM outputs as clock source

跳至解决方案
1,952 次查看
atillametetured
Contributor V


Greetings,

We are designing a custom HW using iMX6Q and one of our peripheral devices needs a clock source of 32.768 kHz. Can we supply this through one of the PWM I/O on iMX? If not what port can I use to supply a peripheral with a clock at this frequency?

Regards,

Mete

标签 (2)
标记 (5)
0 项奖励
回复
1 解答
1,703 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The following may help  i.MX6S CLKO1 does not output 32kHz.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,704 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The following may help  i.MX6S CLKO1 does not output 32kHz.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------