i saw the ./config --help ...searching for some flag that enable the neon intrinsic... and this is the result :
Installation directories:
--prefix=PREFIX install architecture-independent files in PREFIX
[/usr/local]
--exec-prefix=EPREFIX install architecture-dependent files in EPREFIX
[PREFIX]
By default, `make install' will install all the files in
`/usr/local/bin', `/usr/local/lib' etc. You can specify
an installation prefix other than `/usr/local' using `--prefix',
for instance `--prefix=$HOME'.
For better control, use the options below.
Fine tuning of the installation directories:
--bindir=DIR user executables [EPREFIX/bin]
--sbindir=DIR system admin executables [EPREFIX/sbin]
--libexecdir=DIR program executables [EPREFIX/libexec]
--sysconfdir=DIR read-only single-machine data [PREFIX/etc]
--sharedstatedir=DIR modifiable architecture-independent data [PREFIX/com]
--localstatedir=DIR modifiable single-machine data [PREFIX/var]
--libdir=DIR object code libraries [EPREFIX/lib]
--includedir=DIR C header files [PREFIX/include]
--oldincludedir=DIR C header files for non-gcc [/usr/include]
--datarootdir=DIR read-only arch.-independent data root [PREFIX/share]
--datadir=DIR read-only architecture-independent data [DATAROOTDIR]
--infodir=DIR info documentation [DATAROOTDIR/info]
--localedir=DIR locale-dependent data [DATAROOTDIR/locale]
--mandir=DIR man documentation [DATAROOTDIR/man]
--docdir=DIR documentation root [DATAROOTDIR/doc/opencv]
--htmldir=DIR html documentation [DOCDIR]
--dvidir=DIR dvi documentation [DOCDIR]
--pdfdir=DIR pdf documentation [DOCDIR]
--psdir=DIR ps documentation [DOCDIR]
Program names:
--program-prefix=PREFIX prepend PREFIX to installed program names
--program-suffix=SUFFIX append SUFFIX to installed program names
--program-transform-name=PROGRAM run sed PROGRAM on installed program names
System types:
--build=BUILD configure for building on BUILD [guessed]
--host=HOST cross-compile to build programs to run on HOST [BUILD]
--target=TARGET configure for building compilers for TARGET [HOST]
Optional Features:
--disable-FEATURE do not include FEATURE (same as --enable-FEATURE=no)
--enable-FEATURE[=ARG] include FEATURE [ARG=yes]
--enable-static[=PKGS] build static libraries [default=no]
--disable-dependency-tracking speeds up one-time build
--enable-dependency-tracking do not reject slow dependency extractors
--enable-shared[=PKGS] build shared libraries [default=yes]
--enable-fast-install[=PKGS]
optimize for fast installation [default=yes]
--disable-libtool-lock avoid locking (might break parallel builds)
--enable-debug build debug version without optimization [no]
--enable-apps build demo applications [yes]
--enable-sse2 enable SSE2 intrinsics [yes]
--enable-openmp enable OpenMP threading [automatic]
Optional Packages:
--with-PACKAGE[=ARG] use PACKAGE [ARG=yes]
--without-PACKAGE do not use PACKAGE (same as --with-PACKAGE=no)
--with-gnu-ld assume the C compiler uses GNU ld [default=no]
--with-pic try to use only PIC/non-PIC objects [default=use
both]
--with-tags[=TAGS] include additional configurations [automatic]
--with-swig use swig wrapper generator [no]
--with-python use python for wrapping [yes]
--with-octave use octave for wrapping [no]
--with-xine use xine libraries (see LICENSE) [no]
--with-gstreamer use gstreamer multimedia framework (see LICENSE)
[no]
--with-ffmpeg use ffmpeg libraries (see LICENSE) [automatic]
--with-1394libs use libraw1394/libdc1394 [automatic]
--with-v4l use video4linux [automatic]
--with-unicap use unicap (see LICENSE) [no]
--with-imageio use ImageIO libraries [automatic]
--with-quicktime use QuickTime libraries [automatic]
--with-carbon use Carbon windows [automatic]
--with-gtk use gtk+ 2.0 windows [automatic]
--with-gthread use gthread in addition to gtk+ [automatic]
Some influential environment variables:
CXX C++ compiler command
CXXFLAGS C++ compiler flags
LDFLAGS linker flags, e.g. -L<lib dir> if you have libraries in a
nonstandard directory <lib dir>
LIBS libraries to pass to the linker, e.g. -l<library>
CPPFLAGS C/C++/Objective C preprocessor flags, e.g. -I<include dir> if
you have headers in a nonstandard directory <include dir>
CC C compiler command
CFLAGS C compiler flags
CPP C preprocessor
CXXCPP C++ preprocessor
F77 Fortran 77 compiler command
FFLAGS Fortran 77 compiler flags
PYTHON Python Executable Path
SWIG Simplified Wrapper and Interface Generator, used for Python
bindings