Using Internal oscillator for RTC_XTAL in i.MX6 Solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Internal oscillator for RTC_XTAL in i.MX6 Solo

ソリューションへジャンプ
3,051件の閲覧回数
sivaraj
Contributor II

Hi,

We are planning to use internal oscillator instead of connecting external crystal to the RTC_XTAL inputs of iMX6 solo. For enabling internal oscillator, we have connected RTC_XTALI pin to ground and left the RTC_XTALO unconnected.  Can you let me know if any function in i.MX6 can be affected when the i.MX6 is active because of the poor accuracy of the internal oscillator?

Note, We are not planning on using the RTC in our board. The i.MX6 will always be active in our board and no suspend or power down mode implementation is required.

Thanks,

Sivaraj

ラベル(1)
0 件の賞賛
返信
1 解決策
3,035件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes boot issue is fixed for rev.1.3, however if it is used as clock source for gpt, wdog or other

module it is necessary to consider that it may be up to two times faster than a 32 kHz external crystal oscillator.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,038件の閲覧回数
sivaraj
Contributor II

Hi Igor,

We are using i.MX6 processor with silicon revision 1.3 only.

Can you please confirm if there will not be any issues in this due to the internal oscillator accuracy in this Silicon Revision 1.3 and future revisions? 

Thanks,

Sivaraj

0 件の賞賛
返信
3,036件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes boot issue is fixed for rev.1.3, however if it is used as clock source for gpt, wdog or other

module it is necessary to consider that it may be up to two times faster than a 32 kHz external crystal oscillator.

 

Best regards
igor

0 件の賞賛
返信
3,047件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sivaraj

 

for possible issues one can look at ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy..

Chip Errata for the i.MX 6Solo/6DualLite

 

Best regards
igor

0 件の賞賛
返信