Using Internal oscillator for RTC_XTAL in i.MX6 Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Internal oscillator for RTC_XTAL in i.MX6 Solo

Jump to solution
3,007 Views
sivaraj
Contributor II

Hi,

We are planning to use internal oscillator instead of connecting external crystal to the RTC_XTAL inputs of iMX6 solo. For enabling internal oscillator, we have connected RTC_XTALI pin to ground and left the RTC_XTALO unconnected.  Can you let me know if any function in i.MX6 can be affected when the i.MX6 is active because of the poor accuracy of the internal oscillator?

Note, We are not planning on using the RTC in our board. The i.MX6 will always be active in our board and no suspend or power down mode implementation is required.

Thanks,

Sivaraj

Labels (1)
0 Kudos
Reply
1 Solution
2,991 Views
igorpadykov
NXP Employee
NXP Employee

yes boot issue is fixed for rev.1.3, however if it is used as clock source for gpt, wdog or other

module it is necessary to consider that it may be up to two times faster than a 32 kHz external crystal oscillator.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
2,994 Views
sivaraj
Contributor II

Hi Igor,

We are using i.MX6 processor with silicon revision 1.3 only.

Can you please confirm if there will not be any issues in this due to the internal oscillator accuracy in this Silicon Revision 1.3 and future revisions? 

Thanks,

Sivaraj

0 Kudos
Reply
2,992 Views
igorpadykov
NXP Employee
NXP Employee

yes boot issue is fixed for rev.1.3, however if it is used as clock source for gpt, wdog or other

module it is necessary to consider that it may be up to two times faster than a 32 kHz external crystal oscillator.

 

Best regards
igor

0 Kudos
Reply
3,003 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sivaraj

 

for possible issues one can look at ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy..

Chip Errata for the i.MX 6Solo/6DualLite

 

Best regards
igor

0 Kudos
Reply