Using GPT1 in Linux on iMX8MPlus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using GPT1 in Linux on iMX8MPlus

ソリューションへジャンプ
1,589件の閲覧回数
alexeyfirago
Contributor II

Hi all,

We have a custom board based on iMX8MPlus. We want to use GPT1 to capture a signal on SAI3_TXC. We are using kernel revision imx-5.4.47_2.2.0 and revision imx-atf imx_5.4.47_2.2.0.

Is it possible to use GPT1 in Linux? Will adding a DTS node for GPT be enough? Or we also should patch imx8mp_bl31_setup.c in imx-atf?

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,584件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

 

patch was sent via mail.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,585件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

 

patch was sent via mail.

 

Best regards
igor

0 件の賞賛
返信