Using GPT1 in Linux on iMX8MPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using GPT1 in Linux on iMX8MPlus

Jump to solution
2,133 Views
alexeyfirago
Contributor II

Hi all,

We have a custom board based on iMX8MPlus. We want to use GPT1 to capture a signal on SAI3_TXC. We are using kernel revision imx-5.4.47_2.2.0 and revision imx-atf imx_5.4.47_2.2.0.

Is it possible to use GPT1 in Linux? Will adding a DTS node for GPT be enough? Or we also should patch imx8mp_bl31_setup.c in imx-atf?

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
2,128 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

 

patch was sent via mail.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
2,129 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

 

patch was sent via mail.

 

Best regards
igor

0 Kudos
Reply