Using FlexIO to emulate i8080 bus on imx93 Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using FlexIO to emulate i8080 bus on imx93 Linux

356 Views
x10
Contributor V

Hi, NXP TechSupport

I have implemented single beat write / read of i8080 bus cycle on imx93-EVK. The bus timing looks okay with total cycle time 800ns. There is a FASTACC bit in CTRL register, which suppose faster register access. But bus cycle becomes much longer instead of shorter with FASTACC bit enbaled. I suppose I haven't got right way to setup FASTACC bit. Please let me know to use  the function of FASTACC bit in CTRL register. Thanks!

 

Regards

Cheng Shi

0 Kudos
Reply
5 Replies

341 Views
joanxie
NXP TechSupport
NXP TechSupport

for FlexIO to drive 8080 bus, you can refer to the link as below

Using FlexIO to Drive 8080 Bus LCD on K32L2A

for the FASTACC bit, refer to the RM, You must enable the FLEXIO functional clock before accessing any of the FLEXIO registers. Provided the FLEXIO functional clock is at least equal to the bus clock, maybe you need check the functional clock

0 Kudos
Reply

336 Views
x10
Contributor V

As my understanding of RM, the flexio1's functional clock should be flexio1.flexio_clk (RM p.1744), is it right?

For FlexIO DTS :

flexio1: flexio@425c0000 {
compatible = "nxp,imx-flexio";
reg = <0x425c0000 0x10000>;
interrupts = <GIC_SPI 53 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX93_CLK_FLEXIO1_GATE>,
<&clk IMX93_CLK_FLEXIO1_GATE>;
clock-names = "per", "ipg";
assigned-clocks = <&clk IMX93_CLK_FLEXIO1_GATE>;
assigned-clock-parents = <&clk IMX93_CLK_FLEXIO1>;
....
};
 
the flexio functional clock is refered to "IMX93_CLK_FLEXIO1_GATE".
Both ipg_clk and per_clk are enabled in driver's probe function, but FASTACC behaviors weird.
 
Regards
0 Kudos
Reply

285 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the RM, Provided the FLEXIO functional clock is at least equal to the bus clock, the CTRL[FASTACC] field can be set to support fast register accesses., so you also need to check the bus clock

0 Kudos
Reply

277 Views
x10
Contributor V

what is the bus clock in RM? Is it AXI clock or something similar?

0 Kudos
Reply

199 Views
joanxie
NXP TechSupport
NXP TechSupport

bus clock means pclk, this should be the ipg clock, refer to the dts file, it seems the clock is set the same, you also can dump the clocks to check, I didn't find other request for FASTACC enable 

joanxie_0-1756368240235.png

 

0 Kudos
Reply